DOCA0302EN-04

Meters

Overview

The iEM2000T, iEM3110, iEM3155, iEM3210, iEM3255, and iEM3355 products are kilowatt-hour meters from the Schneider Electric range.

Meters not in the Acti 9 range can be controlled by a I/O Smart Link channel. These meters must have the following characteristics:

  • One pulse output

  • Compatibility with standard CEI 62053-31

Wiring

iEM2000T, iEM3110, iEM3155, iEM3210, iEM3255, and iEM3355 kilowatt-hour meters can be connected to channel N (1 ≤ N ≤ 11) of a I/O Smart Link device with an A9XCAU06 or A9XCAC01 pre-wired cable: molded connector (at I/O Smart Link end), and with five wires (at iEM2000T end).

  1. Meter

NOTE: A single I/O Smart Link channel can take account of two meters, one meter on input I1 and 1 meter on input I2.
NOTE:
  • @updatedD8
    A maximum of one wire can be connected in each Ti24 connector terminal (A9XC2412).

  • Do not connect a wire with cable end in each of the Ti24 connector terminals.

Example of Connection of iEM2000T Meters

(1) iEM2000T meter

(2) iEM2000T meter

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?