DOCA0302EN-04

Direct Output Connection

Overview

An indication device or a PLC input can be directly connected to the output (Q) of I/O Smart Link channel.

The connected device should have the following characteristics:

  • To be powered with 24 Vdc

  • The consumption must be less than 100 mA

Wiring

The wiring can be done with an A9XCAU06 or A9XCAC01 pre-wired cable: molded connector (at I/O Smart Link end), and with five wires (at contactor end).

NOTE:
  • @updatedD8
    A maximum of one wire can be connected in each Ti24 connector terminal (A9XC2412).

  • Do not connect a wire with cable end in each of the Ti24 connector terminals.

Example of Connection

(1) Indication light 24 Vdc

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?