Modbus Client/Server Principle
Overview
The Modbus protocol exchanges data using a request/response mechanism between a client and a server. The client/server principle is a type of communication protocol in which a device (the client) controls one or more devices (the servers). A standard Modbus network consists of one client and up to 31 servers.
Characteristics of the Client/Server Principle
The client/server principle has the following characteristics:
-
Only one client at a time is connected to the network.
-
Only the client can launch communication and send requests to servers.
-
The client can address each server individually using its dedicated address or all servers simultaneously using address 0.
-
The servers can only send responses to the client.
-
Servers cannot launch communication with either the client, or the other servers.
Client/Server Communication Modes
The Modbus protocol can exchange data using two communication modes:
-
Request/response mode
-
Broadcast mode
Each I/O Smart Link has a Modbus address (1 to 99), and concentrates data from connected devices on its 11 channels (Ti24 interface).
The states and orders for each device connected to I/O Smart Link are accessible in registers whose address depends on the channel (1 to 11) on which the device is connected.
Request/Response Mode
In request/response mode, the client addresses 1 server using the server dedicated address. The server processes the request, then responds to the client.
Broadcast Mode
In broadcast mode, the client addresses all the servers using address 0. Servers do not respond to broadcast messages.
Turnaround Time
Data Exchange
The Modbus protocol uses two data types:
-
Bits
-
16-bit words called registers
Each register has a register number. Each data type (bit or register) has a 16-bit address.
Messages exchanged with the Modbus protocol contain the address of the data to be processed.
Frames
All frames exchanged with the Modbus protocol are 256 bytes maximum and consist of four fields:
|
Field |
Definition |
Size |
Description |
|---|---|---|---|
|
1 |
Server number |
1 byte |
Destination of the request
|
|
2 |
Function code |
1 byte |
|
|
3 |
|
n bytes |
|
|
4 |
Check |
2 bytes |
CRC16 (to check transmission errors) |
Data Format
The data format is configured as shown in the following table according to Modbus RTU format:
|
Start |
Data |
Parity |
Stop |
|---|---|---|---|
|
1 bit |
8 bits |
1 bit |
1 bit |
Even parity is required, other modes (odd parity, no parity) may be also used.
If no parity is implemented in the Modbus Client, an additional stop bit must be transmitted by the Modbus Client to fill out the character frame to a full 11 bit asynchronous character.