Generating Summary Data Using iOF+SD24 or OF+SD24
Overview
The electrical summary of the SD contacts or summary of the OF contacts can be generated with iOF+SD24 and/or OF+SD24 auxiliaries.
The electrical summary of the OF signals can be done by cabling in series of all OF signals and by connecting this circuit to the I1 input of a channel of I/O Smart Link.
The electrical summary of the SD signals can be done by cabling in series of all SD signals and by connecting this circuit to the I2 input of another channel of I/O Smart Link.
The OF connections (on I1 input) and the SD connections (on I2 input) cannot be connected to the same channel of I/O Smart Link, as the summary information dedicated to the OF signals cannot be separated from the summary information dedicated to the SD signals in I/O Smart Link.
The summary of OF (or SD) signals can be wired in series using the A9XC2412 15-pin connector (spring cage). A maximum of 10 OF (or SD) signals can be wired in the same summary.