System
Serial Number
|
Address |
Register |
No. |
RW |
Type |
Default value |
Svd |
Function code |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x0064 |
101 |
6 |
R |
ASCII |
N/A |
Y |
03, 100-4 |
Serial number on 12 ASCII characters; 11 alphanumeric digits maximum [SN] or [S/N]: PP YY WW [D[nnnn]]
|
Status
|
Address |
Register |
No. |
RW |
Type |
Default value |
Svd |
Function code |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x0070 |
113 |
1 |
R |
BITMAP |
0x0000 |
N |
03, 100-4 |
Status and diagnostic register Bit 0 = 1: start-up phase Bit 1 = 1: operating phase Bit 2 = 1: degraded mode(1) Bit 3 = 1: internal error mode(2) Bit 4: not used Bit 5: not used Bit 6 = 1: invalid data Bit 7 = 1: invalid 24 V I/O Bit 8: not used Bit 9: not used Bit 10: not used Bit 11: not used Bit 12: not used Bit 13: E2PROM error Bit 14: not used Bit 15: EXT FLASH error NOTE: Bits 0 to 3 are exclusive:
only one mode is used at any given time.
|
|
0x0071 |
114 |
1 |
R |
BITMAP |
0xA0CF |
Y |
03, 100-4 |
Validity of the status and diagnostic bit (0 = Invalid / 1 = Valid) – refer to register 113 For example: Address 0 x 0100 — 16 bits register for bit validity of the following register.
|
|
(1) Degraded mode comes into effect:
If a short-circuit on an output has caused a change to degraded mode, at the end of the short-circuit, the output is reset to 0 by the electronics: the Modbus client system sends a Modbus message to reset the output to 1 if it was at 1, before the short-circuit. (2) Internal error mode if an EXT FLASH and/or E2PROM error is detected. The data is invalid in the start-up phase, degraded and internal error modes. Invalid data include inputs 1 and 2, the power or flow indicator, the operation and running hours counter.
|
||||||||
Date and Time
|
Address |
Register |
No. |
RW |
Type |
Range |
Default value |
Svd |
Function code |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x0073 |
116 |
4 |
RW |
DATE |
(1) |
N/A |
N |
03, 16, 100-4 |
Indicates the year, month, day, hour, minute and millisecond on the I/O Smart Link device. |
|
(1) See description of the DATETIME type. |
|||||||||
Hardware and Firmware Versions
|
Address |
Register |
No. |
RW |
Type |
Default value |
Svd |
Function code |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x0086 |
135 |
6 |
R |
ASCII |
N/A |
Y |
03, 100-4 |
Hardware version on 11 ASCII characters. Example: 002.000.000 |
|
0x008C |
141 |
6 |
R |
ASCII |
N/A |
Y |
03, 100-4, 43-14 |
Firmware version on 11 ASCII characters. Example: 003.002.001 |
|
0x0092 |
147 |
6 |
R |
ASCII |
N/A |
Y |
03, 100-4 |
Boot firmware version on 11 ASCII characters. Example: 001.032.000 |
Identification
|
Address |
Register |
No. |
RW |
Type |
Default value |
Svd |
Function code |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x01F4 |
501 |
8 |
R |
ASCII |
EcoStruxure |
N/A |
|
Product range |
|
0x01FC |
509 |
8 |
R |
ASCII |
I/O Device |
N/A |
|
Product family |
|
0x0204 |
517 |
32 |
R |
ASCII |
N/A |
|
Vendor URL |
|
|
0x0224 |
549 |
8 |
R |
ASCII |
I/O Smart Link |
N/A |
|
Product model |
|
0x022C |
557 |
1 |
R |
UINT16 |
9100 |
N/A |
|
Product identifier |
|
0x022D |
558 |
16 |
R |
ASCII |
Schneider Electric |
N/A |
|
Vendor name |
|
0x023D |
574 |
10 |
RW |
ASCII |
I/O Smart Link |
Y |
|
User application name |
|
0x0247 |
584 |
16 |
R |
ASCII |
A9XMSB11 |
N/A |
|
Commercial reference |
|
0x0257 |
600 |
10 |
R |
ASCII |
I/O |
N/A |
|
Product capability |