Other Devices
Description
Devices that can be connected to the I/O Smart Link are:
-
Meter with a pulse output and compliant with standard IEC 62053-31
-
Volt-free low level indication contact
-
Volt-free standard indication contact
-
Contactor and relay
-
Indication device or PLC input can be directly connected to the output (Q) of I/O Smart Link channel.
The connected device should have the following characteristics:
-
To be powered with 24 Vdc
-
The consumption must be less than 100 mA
-
-
Any device (for example, motor) that needs a command circuit of more than 100 mA can be controlled by the output (Q) of a channel of I/O Smart Link. The electrical diagram must be indirect between I/O Smart Link and this device: a low level relay must be installed between the command of this device and I/O Smart Link.