DOCA0302EN-04

Contactor and Relay (Not in the Acti 9 Range)

Overview

A contactor or relay powered with 24 Vdc can be connected to I/O Smart Link. This should have the following characteristics:

  • The contactor or relay coil must not draw more than 100 mA

  • The indication contact must be low level type

Only contactors in the Acti 9 range can be connected to I/O Smart Link using the iACT24 auxiliary.

Wiring

A contactor can be connected with an A9XCAU06 or A9XCAC01 pre-wired cable: molded connector (at I/O Smart Link end), and with five wires (at contactor end).

@writer : set trans_SLMB_0000828162.eps to TRANS
NOTE:
  • @updatedD8
    A maximum of one wire can be connected in each Ti24 connector terminal (A9XC2412).

  • Do not connect a wire with cable end in each of the Ti24 connector terminals.

Example of Connection

(1) Low level relay (for example, iRBN)

(2) 24 Vdc relay

(3) Power contactor (for example, TeSys Deca LC1D••••)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?