Modbus Table Format and Data Types
Table Formats
Register tables have the following columns:
|
Address |
Register |
No. |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Function code |
Description |
|
Designation |
Description |
|---|---|
|
Address |
16-bit register address in hexadecimal. The address is the data used in the Modbus frame. |
|
Register |
16-bit register number in decimal. Register = Address + 1 |
|
No. |
Number of 16-bit registers that need to be read/written to access the complete information. |
|
RW |
Whether the register is read only (R) or read-write (RW). |
|
X |
Scale factor:
|
|
Unit |
Information unit of measurement:
|
|
Type |
Coding data type (see Data types table). |
|
Range |
Range of permitted values for the variable, usually a subset of what the format allows. For BITMAP type data, the content of this domain is "–". |
|
Default value |
Default value for the variable. |
|
Svd |
Saving the value in the event of a power failure:
NOTE: On start-up or reset, the available values
are retrieved.
|
|
Function code |
Code of functions that can be used in the register. |
|
Description |
Information about the register and the restrictions that apply. |
Data Types
The following data types appear in the tables of Modbus registers:
|
Name |
Description |
Range |
|---|---|---|
|
UINT |
16-bit unsigned integer (1 word) |
0 to 65535 |
|
INT |
16-bit signed integer (1 word) |
-32768 to +32767 |
|
UINT32 |
32-bit unsigned integer (2 words) |
0 to 4 294 967 295 |
|
INT32 |
32-bit signed integer (2 words) |
-2 147 483 648 to +2 147 483 647 |
|
Float32 |
32-bit value (2 words) |
-3.4028E+38 to +3.4028E+38 |
|
ASCII |
8-bit alphanumeric character |
Table of ASCII Characters |
|
BITMAP |
16-bit field (1 word) |
– |
|
DATE |
See Date table |
– |
Float32 type data: Single precision float with sign bit, 8 bits exponent, 23 bits mantissa (positive and negative normalized real)
For ASCII type data, the order of transmission of characters in words (16-bit registers) is as follows:
-
Character n as least significant
-
Character n + 1 as most significant
All registers (16-bit or 2 bytes) are transmitted with Big Endian coding:
-
The most significant byte is transmitted first
-
The least significant byte is transmitted second
32-bit variables saved on two 16-bit words (for example, consumption meters) are in Big Endian format:
-
The most significant word is transmitted first, then the least significant.
64-bit variables saved on four 16-bit words (for example, dates) are in Big Endian format:
-
The most significant word is transmitted first, and so on.
DATETIME
DATETIME is a data type used to code date and time defined by the IEC 60870-5 standard.
|
Register |
Type |
Bit |
Range |
Description |
|---|---|---|---|---|
|
1 |
INT16U |
0–6 |
0x00–0x7F |
Year: 0x00 (00) to 0x7F (127) correspond to years 2000 to 2127 For example, 0x17 (23) corresponds to year 2023. |
|
7–15 |
– |
Reserved |
||
|
2 |
INT16U |
0–4 |
0x01–0x1F |
Day |
|
5–7 |
– |
Reserved |
||
|
8–11 |
0x00–0x0C |
Month |
||
|
12–15 |
– |
Reserved |
||
|
3 |
INT16U |
0–5 |
0x00–0x3B |
Minutes |
|
6–7 |
– |
Reserved |
||
|
8–12 |
0x00–0x17 |
Hours |
||
|
13–15 |
– |
Reserved |
||
|
4 |
INT16U |
0–15 |
0x0000–0xEA5F |
Milliseconds |
Direct Bit Addressing
Addressing is permitted for BITMAP type zones with functions 1, 2, 5 and 15.
The address of the first bit is constructed as follows: (register address x 16) + bit number.
This addressing mode is specific to Schneider Electric.
Example: For functions 1, 2, 5 and 15, bit 3 of register 0x0078 should be addressed; the bit address is therefore 0x0783.
Example of Modbus Frames
Request
|
Definition |
Number of Bytes |
Value |
Comment |
|---|---|---|---|
|
Server number |
1 byte |
0x05 |
I/O Smart Link Modbus address |
|
Function code |
1 byte |
0x03 |
Reads n output or internal words |
|
Address |
2 bytes |
0x36E2 |
Address of a consumption meter whose address is 14050 in decimal notation. |
|
Number of words |
2 bytes |
0x002C |
Reads 44 16-bit registers. |
|
CRC |
2 bytes |
xxxx |
Value of CRC16. |
Response
|
Definition |
Number of Bytes |
Value |
Comment |
|---|---|---|---|
|
Server number |
1 byte |
0x05 |
I/O Smart Link Modbus address |
|
Function code |
1 byte |
0x03 |
Reads n output or internal words |
|
Number of Bytes |
2 bytes |
0x0058 |
Number of bytes read |
|
Value of words read |
88 bytes |
– |
Reads 44 16-bit registers |
|
CRC |
2 bytes |
xxxx |
Value of CRC16. |
Modbus Address
The list of Modbus addresses, defined by the Modbus protocol, starts at 0.
The address of register number n is n-1.
The detailed tables in subsequent chapters of this guide provide both register numbers (in decimal format) and corresponding addresses (in hexadecimal format). Example of address: address of register number 3000 is 0x0BB7 (2999).