DOCA0302EN-04

Acti 9 Devices with Ti24 Interface

Description

Devices that can be connected to the I/O Smart Link are listed in the following table:

Device

Product Reference

Description

iACT24 auxiliary for iCT contactor

A9C15924

The iACT24 auxiliary:

  • allows control and indication of a 230 Vac contactor iCT rated 25 A or higher from the I/O Smart Link by 24 Vdc signals (Y3),

  • allows control by a maintained signal (Y2),

  • is used to find out the contactor status (O/C status).

iATL24 auxiliary for iTL contactor

A9C15424

The iATL24 auxiliary:

  • allows control and indication of a 230 Vac impluse relay iTL from the I/O Smart Link by 24 Vdc signals (Y3),

  • allows control by a pulsed signal (Y2),

  • is used to find out the impulse relay status (O/C status).

iOF+SD24 indication auxiliary for iC60, iC40, iDPN, iCV40 and iID, iID40, and iSW-NA

A9A26897

Compatible with downstream comb busbar, the iOF+SD24 indication auxiliary is used to find out the status (OF) and the tripping status upon a fault () of iC60, iC40, iDPN, iCV40 and iID, iID40, and iSW-NA.

iOF+SD24 indication auxiliary for iC60, iC40, iDPN, iCV40 and iID, iID40, and iSW-NA

A9A26898

Compatible with upstream comb busbar, the iOF+SD24 indication auxiliary is used to find out the status (OF) and the tripping status upon a fault () of iC60, iC40, iDPN, iCV40 and iID, iID40, and iSW-NA.

OF+SD24 indication auxiliary for C60, C120, DPN, DPN Vigi, C60H-DC and ID, SW60-DC, C60PV-DC, C60NA-DC, and C120NA-DC

A9N26899

Compatible with downstream comb busbar, the OF+SD24 indication auxiliary is used to find out the status (OF) and the tripping status upon a fault () of the following devices: C60, C120, DPN, DPN Vigi, C60H-DC and ID, SW60-DC, C60PV-DC, C60NA-DC, and C120NA-DC.

iOF/SD24 indication auxiliary for iC60 RCBO

A9A19804

Compatible with downstream comb busbar, the iOF/SD24 indication auxiliary is used to find out the status (OF) or the tripping status upon a fault () of the iC60 RCBO.

Acti 9 RCA iC60 remote control with Ti24 interface

A9C7012•

The Acti 9 RCA iC60 remote control:

  • Should have a Ti24 interface (with product references A9C70122 and A9C70124).

  • Can be used to control an iC60 circuit breaker via input Y1/Y2 local control depending on the selected mode and Y3 of its Ti24 interface. Input Y3 (24 Vdc) can be controlled by one of the I/O Smart Link channels.

  • Can be used to find out the OF and status of the circuit breaker associated with the RCA iC60 remote control.

Acti 9 Reflex iC60 integrated control circuit breaker with Ti24 interface

A9C6••••

The Acti 9 Reflex iC60 integrated control circuit breaker:

  • Should have a Ti24 interface (with product references A9C6••••).

  • Can allow the device to be controlled via input Y3 of its Ti24 interface. The Y3 (24 Vdc) input can be controlled by one of the I/O Smart Link channels.

  • Can be used to indicate the state of the control circuit (O/C) and circuit breaker state (auto/OFF).

NOTE: All the devices in the preceding table can be connected to channel N (1 ≤ N ≤ 11) of a I/O Smart Link device with A9XCAS06 pre-wired cable (or A9XCAM06 or A9XCAH06).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?