EcoStruxure Power Commission Software
Overview
EcoStruxure Power Commission is an all-in-one software tool used to configure, test, and provide reporting for smart devices in your electrical equipment.
EcoStruxure Power Commission software offers a quick test process based on a very intuitive Graphical User Interface.
This software has the ability to deal with multiple I/O Smart Link devices at the same time. They can be chained and multiple Acti 9 devices can be connected to the computer using Smart Link Modbus and Panel Server network. The maximum number of I/O Smart Link devices that can be connected for Modbus network is 10. The maximum number of I/O Smart Link server devices that can be connected for Panel Server network is eight. The server devices can include I/O Smart Link.
EcoStruxure Power Commission software is used to update the I/O Smart Link firmware. For more information, see EcoStruxure Power Commission Online Help.
The I/O Smart Link can only be updated through IFE Ethernet interface or Panel Server.
When I/O Smart Link firmware upgrade is initiated, the I/O Smart Link device should be in an isolated network along with the gateway. No other Modbus client should be polling any other Modbus device connected in the same network.
Main Functions
EcoStruxure Power Commission software has four main functions:
-
Testing the installation
-
Generating test reports
-
Upgrading the firmware version of I/O Smart Link
-
Configuring the Acti 9 devices connected to I/O Smart Link and recovering the configuration of I/O Smart Link channels
In order to test the installation, the software:
-
Tests the communication network (Modbus SL/Modbus TCP/IP).
-
Tests the connection and the status of the electrical devices connected to I/O Smart Link.
Also, the software provides the following reports:
-
List of tested devices (.pdf and .xlsx files)
-
I/O Smart Link channels assignment (.dxf file)
Downloading and Installing EcoStruxure Power Commission Software
To download and install EcoStruxure Power Commission software, refer to DOCA0134EN EcoStruxure Power Commission Installation Guide.
Commissioning with EcoStruxure Power Commission Software
To commission I/O Smart Link, refer to the EcoStruxure Power Commission Online Help.
Firmware Update with EcoStruxure Power Commission Software
For more information about firmware update refer DOCA0303EN EcoStruxure I/O Smartlink Firmware Release Note.