Overview
Overview
All the Modbus tables in the I/O Smart Link device have been designed to minimize the number of Modbus requests that the client system needs to send in order to collect the data prepared by I/O Smart Link.
The Modbus tables in the I/O Smart Link device are compact and are summaries of all the data collected on the 11 channels of the I/O Smart Link device.
The Modbus tables in the I/O Smart Link device are described in:
-
The section presenting:
-
The section presenting the address zones for each type of device that can be connected to I/O Smart Link: iOF+SD24, OF+SD24, iACT24, iATL24, RCA iC60, Reflex iC60, iEM2000T, meter, contactor and impulse relay
-
The section presenting the address zones for each type of data (status, orders, measurements and parameter settings) with a description of the summary zones and a description of the detailed data zones for each channel.
General Organization of Modbus Tables in I/O Smart Link Devices
|
Item |
Description |
See |
|---|---|---|
|
1 |
Channel summary data |
|
|
2 |
System data independent of the channel |
|
|
3 |
Data for channel 1 Devices that can be connected to channel 1 |
|
|
4 |
Data for channel 2 to 11 Devices that can be connected to channel 2 to 11 |