Modbus Functions
General Description
The Modbus protocol offers functions for reading or writing data on the Modbus network. This protocol also offers diagnostic and network management functions.
Only Modbus functions managed by the I/O Smart Link device are described here.
Table of Modbus Functions
The following table describes in detail the functions supported by I/O Smart Link devices:
|
Function code |
Sub-Function code |
Function Name |
|---|---|---|
|
01 |
– |
Read n output or internal bits |
|
02 |
– |
Read n input bits |
|
03 |
– |
Read n output or internal words |
|
05 |
– |
Write 1 bit |
|
06 |
– |
Write 1 word |
|
08 |
(1) |
Modbus diagnostics |
|
15 |
– |
Write n bits |
|
16 |
– |
Write n words |
|
43 |
14(2) |
Read identification |
|
15(3) |
Read the date and time |
|
|
16(4) |
Write the date and time |
|
|
100 |
4(5) |
Read n non-adjacent words where n ≤ 100. NOTE: Thanks to the read distributed
holding register function, the user can:
|
|
(1) For more details, see the appendix describing function 8 (2) For more details, see the appendix describing function 43–14 (3) For more details, see the appendix describing function 43-15 (4) For more details, see the appendix describing function 43-16 (5) For more details, see the appendix describing function 100-4 |
||