DOCA0302EN-04

Volt-Free Standard Indication Contact

Overview

A standard indication contact (NO or NC) can be connected to input I1 or I2 of a I/O Smart Link channel.

NOTE: A single I/O Smart Link channel can take account of two indication contacts, one contact on input I1 and one contact on input I2. The electrical diagram must be indirect between I/O Smart Link and this device: a low level relay must be installed between the contact of this device and I/O Smart Link.

Wiring

An indication contact can be connected with an A9XCAU06 or A9XCAC01 pre-wired cable: molded connector (at I/O Smart Link end), and with the five wires (indication contact end).

NOTE:
  • @updatedD8
    A maximum of one wire can be connected in each Ti24 connector terminal (A9XC2412).

  • Do not connect a wire with cable end in each of the Ti24 connector terminals.

Example of Connection

(1) NG125 circuit breaker: OF+SD auxiliary contacts with a minimum current of 100 mA

(2) iRBN relay for OF signal

(3) iRBN relay for SD signal

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.