DOCA0302EN-04

Indirect Output Connection

Overview

Any device (for example, a motor) that needs a command circuit of more than 100 mA can be controlled by the output (Q) of a channel of I/O Smart Link. The electrical diagram must be indirect between I/O Smart Link and this device: a low level relay must be installed between the command of this device and I/O Smart Link.

Wiring

The wiring can be done with an A9XCAU06 or A9XCAC01 pre-wired cable: molded connector (at I/O Smart Link end), and with five wires (at contactor end).

NOTE:
  • @updatedD8
    A maximum of one wire can be connected in each Ti24 connector terminal (A9XC2412).

  • Do not connect a wire with cable end in each of the Ti24 connector terminals.

Example of Connection

(1) Relay iRTBT

(2) Contactor Tesys D LC1D•25 with an 230 Vac coil

(3) Motor 10 kW (13.41 hp) with power supply 3-phases 380 Vac

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?