PowerLogic P3 Range

The PowerLogic P3 Range

PowerLogic P3 Standard

PowerLogic P3 Advanced

Features and Benefits

  • Simplified configuration with the new eSetup Pro setting tool

  • Faster delivery with on-the-shelf availability of standard configurations

  • Simpler operation and maintenance with the Schneider Electric Power Device App

  • Native support for a wide range of communication protocols: IEC 61850, Modbus TCP/IP, Modbus RTU, DNP 3.0, SPA-bus, IEC 60870-5-101, IEC 60870-5-103, ProfibusDP, and DeviceNet

  • Embedded arc protection

  • Built-in virtual injection testing

  • Compliant with international standards


Refer to catalog NRJCAT17764EN for the PowerLogic P3 Series.

Feedback