PowerLogic P5 Range

The PowerLogic P5 Range

Features and Benefits

  • Built-in Arc flash protection

  • Increased number of inputs and outputs for more possibilities

  • Compliance to IEC62443 SL1 cybersecurity standard

  • Nearby control via mobile app and embedded web-server

  • Withdrawable design with secured CT connections while drawn-out

  • Nine communication protocols out of the box

  • Natively compliant to IEC61850 standard

  • Modular design for communication port options and back-up memory

  • Low Power Current Transformer (LPCT) / Voltage Transformer (LPVT) compatible

  • Powerful logic configuration

  • Built-in virtual injection testing


Refer to catalog NRJED313567EN for the PowerLogic P5 Series.


Feedback