Assembly of Forced Cooling Fan
CAUTION |
|---|
|
HAZARD of incorrect assembly
Failure to follow these instructions can result in injury or equipment damage.
|
Follow the below procedure for tunnel and forced cooling fan assembly:
Assembly of the Frame (Support plates, Frame, and Rear sheets):
-
Assemble the rear frame support plate A (2) with the two M8 x 25 bolts (1) and two M6 x 8 bolts (3).
-
Assemble the rear frame support plate B (4) with the two M8 x 25 bolts (1) and two M6 x 8 bolts (3).
-
Assemble the rear frame support plate C (5) with the seven M6 x 8 bolts (6).
1
M8 x 25 bolts
4
Support plate B
2
Support plate A
5
Support plate C
3
M6 x 8 bolts
6
M6 x 8 bolts
-
Assemble both the frames (1) with the 44 M6 bolts (4).
NOTE: Use M6 x 12 bolts for two sheet metal plates joint (3) and
M6 x 16 bolts for three sheet metal plates joint (2).1
Frames
3
Two sheet metal plates joint
2
Three sheet metal plates joint
4
M6 bolts
-
Assemble the rear sheet (2) with the 24 M6 x 12 bolts (1).
1
M6 x 12 bolts
2
Rear sheet
Assembly of the ventilation channel:
-
Insert the 16 M6 rivet nuts (3) on the air ventilation channel using a rivet gun.
NOTE: Follow the above step only if the rivet/insert nuts are not installed to the panel. -
Pre-assemble the air ventilation channel to the front plate (2) of the gas tunnel using eight M6 x 12 bolts (1).
1
M6 x 12 bolts
2
Front plate
3
M6 rivet nuts
-
Before starting the assembly, insert the two M6 rivet nuts (2) on the front lifting brackets (1) using a rivet gun.
NOTE: Follow the above step only if the rivet/insert nuts are not installed to the panel. - To install the ventilation channel:
-
Insert the ventilation channel (1) from the top of the cubicle into the circuit breaker compartment.
1
Ventilation channel
2
Pressure relief flap
NOTICE HAZARD OF INAPPROPRIATE ASSEMBLYDuring the insertion of the ventilation channel, coordinate the pressure relief flap to their functional positions.Ensure the ventilation channel should not collide with the pressure relief flap during its insertion.Failure to follow these instructions can result in equipment damage.NOTE: In case an arc sensor (1) is present, the sensor cable can be routed through the hole (2) in the front plate (3), refer to below figure view A. Without the sensor, the cover should be flipped, which closes the hole (2) completely, refer to below figure view B. -
Fix the ventilation channel to the front lifting brackets (1) of the cubicle with four M6 x 16 bolts (2) two each on either side.
-
Assembly of the tunnel:
Pre-assemble the AAVS (1) with the twelve M6 x 16 bolts (3) and the fan’s IP grid (4) with the four M6 x 16 bolts (5) to the top plate (2) of the gas tunnel.
|
1 |
AAVS |
4 |
IP grid |
|
2 |
Top plate |
5 |
M6 x 16 bolts |
|
3 |
M6 x 16 bolts |
Assembly of the top plate:
Assemble the top plate (1) with the 27 M6 x 12 bolts (2).
|
1 |
Top plate |
|
2 |
M6 x 12 bolts |
Assembly of the fan assembly:
-
Remove the four M6 x 16 bolts (1) from the IP grid (2) to mount the fan on top equipped plate on the IP grid.
1
M6 x 16 bolts
2
IP grid
-
Place the rectangular frame on top of IP grid.
-
Mount the fan assembly (1) on the gas duct from the front of the cubicle.
-
Install the fan assembly (1) with a total of eight M6 x 16 bolts (2), four on the front and two each on either side.
CAUTION