BRU8628300-00

Number of Forced Cooling Fans

To provide extra cooling, only one fan is required. An additional fan is installed alongside the first one as a standby, in case of any potential fan malfunction.

An automatic or manual change-over switch is provided in the control circuit to easily switch between the operational fan and the standby fan.

Figure 6
Number of Forced Cooling Fans

1

Standby status (in operation)

2

Reserved status

3

Invertible / Removable plate airflow block

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?