BRU8628300-00

Fan Control Wiring

NOTE: The fan control has a plug with five sockets for the five cables. It has a connection in the low voltage cabinet.

Follow the below steps to connect the fan control wiring:

  1. Remove the five cables from the plug.

  2. Pass all the five cables through the rubber band on top of the low-voltage compartment.

  3. Reconnect the five cables to the plug.

  4. Connect the plug to its counterpart inside the low-voltage compartment.

    NOTE: The plugs are named on the current line drawings, naming can differ based on the project.

    Wiring table

    LV Compartment:

    - X51

    - X52

    - X53

    - X54

    - X55

    FAN-1

    FAN-1:L

    :22

    -

    -

    -

    -

    FAN-1:N

    -

    :12

    -

    -

    -

    FAN-2

    FAN-2:L

    -

    -

    :22

    -

    -

    FAN-1:N

    -

    -

    -

    :12

    -

    Earthing

    FAN-1, 2:E

    -

    -

    -

    -

    :12

    NOTE: The above shown pictures are for representation only, and they may differ from the actual products.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?