BRU8628300-00

Technical Description

Description

Value

Size

225 mm

Leakage current

< 0.75 mA

Operation mode

Continuous operation (S1)

Direction of rotation

Counter-clockwise, seen on rotor

Insulation class

B

Bearing motor

Ball bearing

Mass

12.5 kg

Housing material

Sendzimir galvanized sheet steel

Material of impeller

Sendzimir galvanized sheet steel

Motor protection

Thermal Overload Protector (TOP) wired internally

Type of Protection

IP54

Protection class

I

Figure 3
Airflow Charts

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?