BRU8628300-00

Storage

WARNING
HAZARD OF STORING UNDER INADEQUATE CONDITIONS
Ensure that the storage area is even and supporting area provides sufficient stability.
Ensure that the specified storage conditions are met.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
NOTICE
HAZARD OF STORING UNDER INADEQUATE CONDITIONS
Comply with the storing time before installation is compliant with the warranty period in the terms and conditions.
Storage only in packed condition. Performance will not be guaranteed if stored in open condition.
Failure to follow these instructions can result in equipment damage.

If the panels are not installed immediately after delivery, they can be stored under the following conditions:

  • Indoor storage only is admissible.

  • Fans and accessories can be stored sealed with desiccants in aluminum foil and packed in a wooden box.

  • Pallet is not removed before/until installation.

  • The storage room environment must be healthy, no rodents, humidity control ≤ 95%/≤ 90% for 24 hours and 1 month respectively, and no water on the floor.

Figure 4
Indoor Storage of the Forced Cooling Fan

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?