BRU8628300-00

Disposal

For Schneider Electric, environmental protection and resource preservation are part of our core corporate goals. Schneider Electric operates an environmental management system which is certified in accordance with ISO 14001 and rigorously implemented around the world based on German standards.

Right from the development stage, ecological design, technical safety, and health protection are fixed criteria.

The following section contains recommendations for ecological disposal of the product and its components.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?