Screw Fastenings
CAUTION |
|---|
|
HAZARD OF INAPPROPRIATE ASSEMBLY
During the assembly, always use the tightening torque
values mentioned in the table below.
Failure to follow these instructions can result in injury or equipment damage.
|
The following elements should be used for all screw fastenings:
-
Screws and bolts: Grade ≥ 8.8
-
Nuts: Grade 8
|
Hex, bolts,
socket-head cap screws (except slotted screws), and nuts (except |
||
|---|---|---|
|
Thread size |
Tightening torque (N•m) |
|
|
Min. |
Max. |
|
|
M5 |
3.8 |
4.7 |
|
M6 |
7 |
9 |
|
M8 |
16 |
24 |
|
M10 |
36 |
44 |
|
M12 |
63 |
77 |
|
Screw fastening with casting nuts in cast resin parts (transformer and post insulator) |
||
|---|---|---|
|
Thread size |
Tightening torque (N•m) |
|
|
Min. |
Max. |
|
|
M6 |
5 |
7.5 |
|
M8 |
12 |
18 |
|
M10 |
24 |
38 |
|
M12 |
63 |
54 |
|
Screw fastening for current transmission conductor material is copper |
||
|---|---|---|
|
Thread size |
Tightening torque (N•m) |
|
|
Min. |
Max. |
|
|
M6 |
5.5 |
7.5 |
|
M8 |
12 |
19 |
|
M10 |
30 |
40 |
|
M12 |
60 |
76 |
CAUTION