BRU8628300-00

Integrated Protective Features

The integrated protective features are designed to automatically switch off the motor in case of any detected faults.

For details, refer to the table below.

Detected fault

Safety feature description/function

Rotor position detection error

An automatic restart follows.

Blocked rotor

After the blockage is removed, the motor restarts automatically.

Line under voltage (line voltage outside of permitted nominal voltage range)

If the line voltage returns to permitted values, the motor restarts automatically.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?