Safety Provisions
Read the following instructions carefully before working on the fan, and perform the work detailed in them as described. Do not perform any work which is not described in this guide.
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
WARNING |
|---|
|
Hazard of Electric shock, explosion or arc flash
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
Applicable Standards and Regulations
The applicable standards and regulations are as follows:
-
Adjustable speed electrical power drive systems (Safety requirements - Electrical, thermal and energy): EN 61800-5-1.
-
Adjustable speed electrical power drive systems (Generic interface for power drive systems - Communication and control): EN 61000-6-2.
-
Electromagnetic compatibility (EMC).
(Generic standards - Emission standard for residential, commercial, and light-industrial environments): EN 61000-6-3.
Electromagnetic Compatibility (EMC)
The applicable EMC standards are as follows:
-
EMC immunity to interference: EN 61000-6-2.
-
EMC circuit feedback: EN 61000-3-2/3.
DANGER
WARNING