BRU8628300-00

Nameplate

The type designation on the nameplates on the front of the panels (Figure 2) informs about essential technical data. When submitting enquiries to the manufacturer or ordering spare parts, the following information is required:

  • Type designation

  • Serial number

  • Year of construction

Figure 2
Nameplate on Panel Front

A

Type designation

C

Year of construction

B

Serial number

D

Technical data

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?