BRU8628300-00

Disassembly of Forced Cooling Fan

WARNING
HAZARD OF INAPPROPRIATE HANDLING
  • Some of the product components are heavy. Make sure that the components do not drop off during disassembly, this can result in fatal or serious injury and material damage.
  • Secure components before unfastening to stop them falling.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
CAUTION
HAZARD OF INAPPROPRIATE DISASSEMBLY
  • Disassembly of the product must be performed or supervised by qualified personnel with the appropriate technical knowledge.
  • The product is to be disassembled into suitable components for disposal employing standard procedures for motors.
Failure to follow these instructions can result in injury or equipment damage.
NOTE: The product should be disassembled into appropriate components for disposal, following standard procedures for motors.

Follow the below steps to disassemble the entire fan assembly and the tunnel:

  1. Disconnect all the wires if the fan with alarms, condensator and all other components to which the fan is connected.

  2. Follow the steps in reverse order of forced cooling fan assembly procedure for the disassembly, refer to Assembly of Forced Cooling Fan.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?