BRU8628300-00

Switching OFF the Forced Cooling Fan

Switching OFF the forced cooling fan during operation:

  • Switch OFF the forced cooling fan via the control input.

  • Do not switch ON and switch OFF the motor (for example in cyclic operation) through power supply.

Switching OFF the forced cooling fan for maintenance:

  • Switch OFF the forced cooling fan via the control input.

  • Do not switch ON and switch OFF the motor (for example in cyclic operation) through power supply.

  • Disconnect the forced cooling fan from the power supply.

  • When disconnecting, also disconnect the ground earthing.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?