BRU8628300-00

Checking Connections

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Make sure that there is isolation from supply (all phases).
  • Make sure that the restart is impossible.
  • Check for all the cables for proper fit.
Failure to follow these instructions will result in death or serious injury.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?