BRU8628300-00

Electrical Connection

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Comply with the safety precautions. Refer to Safety Precautions.
  • Apply appropriate PPE and follow safe electrical work practices. See standards or local equivalent.
  • Before working on the electrical hookup, short the supply and earthing connections.
  • Ensure all the earthing connections that are essential for electrical current to safely ground in the event of a system fault or overload.
  • Check for the correct earthing.
Failure to follow these instructions will result in death or serious injury.
DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Only use the cables that meet the specified installation regulations for voltage, current, insulation material, capacity, and so on.
  • Ensure that the cables are routed so they do not come into contact with any rotating parts.
Failure to follow these instructions will result in death or serious injury.
DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Ensure the device is a built-in component and has no disconnecting switch.
  • Only connect the device to circuits that can be switched OFF with an all-pole disconnection switch.
  • When working on the device, secure the system/machine in which the device is installed to help prevent it from being switched ON back.
Failure to follow these instructions will result in death or serious injury.
CAUTION
HAZARD OF INAPPROPRIATE USE CONDITIONS
Ensure that there is no water ingress into wires or cables, as water entry from customer's connection points can damage the device.
Ensure that the end of the cable is connected in a dry environment.
Failure to follow these instructions can result in injury or equipment damage.

Electrical charge (>50 μC) between phase conductor and earthing connection after switching OFF supply with multiple devices connected in parallel.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?