BRU8628300-00

Replacement

WARNING
HAZARD OF INAPPROPRIATE HANDLING
  • Some of the product components are heavy. Make sure that the components do not drop off during disassembly, this can result in fatal or serious injury and material damage.
  • Secure components before unfastening to stop them falling.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Replacement of the product must be performed or supervised by qualified personnel with the appropriate technical knowledge.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?