BRU8628300-00

Requirements

WARNING
hazard due to overheating
  • The earthing must have a cross-section equal to or greater than that of the phase conductor.
  • Ensure that only 105 °C cables are used to avoid overheating.
  • Make sure that the minimum cable cross-section is at least
    AWG 26/0.13 mm2.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Check the following before connecting the device:

  • Nameplate matches the connection data.

  • Power supply matches the device voltage.

  • Cables used are designed for the current level indicated on the nameplate.

For determining the cross-section:

  • Make sure the sizing criteria is according to EN 61800-5-1:

    • The resistance requirements for both the earthing connection circuit and the customer earthing connection points should comply with the indicated standard.

    • Depending on the installation condition, it may be necessary to connect an additional earthing conductor through the extra earthing terminal provided on the device.

    • The earthing terminal is located on the housing and provided with an earthing symbol and a hole.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?