BRU8628300-00

Electromagnetic Compatibility (EMC)

The applicable EMC standards are as follows:

  • EMC immunity to interference: EN 61000-6-2.

  • EMC circuit feedback: EN 61000-3-2/3.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?