BRU8628300-00

Troubleshooting - Double Fan Malfunction

For the extra cooling details, refer to Number of Forced Cooling Fans.

Invert a removable selective tray to enable the airflow from the stand-by fan and block the other one. For detailed instructions, refer to Switching the Active Cooling Fan (in case of Double Fan).

This system suggests fast fan-stand-by recovery, and replacing the malfunction fan can be made while the other fan is in stand-by status without shutting down the panel with respect to the local protective measures.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?