BRU8628300-00

Locked-Rotor Protection

NOTE: Due to the locked-rotor protection, the starting current that is Locked Rotor Amperage (LRA) is equal to or less than the nominal current that is Full Load Amperage (FLA).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?