BRU8628300-00

Cables Connection

The device has external leads:

  • Connect the earthing.

  • Connect the cables according to the application. For more details, refer to Connection Diagram.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?