About the Document
Intended Use
DANGER |
|---|
|
Hazard of electric shock, explosion or arc flash
Do not operate the forced cooling fan in the following
ways:
Failure to follow these instructions will result in death or serious injury.
|
WARNING |
|---|
|
HAZARD OF INAPPROPRIATE USE CONDITIONS
Any other usage above and beyond this, does not comply
with the intended purpose and constitutes misuse of the forced cooling
fan.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
The forced cooling fan is exclusively designed as a built-in forced cooling fan for conveying air according to its technical data.
Customer equipment must be capable of withstanding the mechanical and thermal stresses that may arise from this product.
This applies for the entire service life of the equipment in which this product is installed.
All dimensions not specified in detail are in millimeters.
Intended use also includes:
-
Use of the forced cooling fan in stationary systems only.
-
Performance of all maintenance work.
-
Conveying air is always at an ambient air pressure.
-
Using the forced cooling fan within the permitted ambient temperature range, refer to Transport and Electromagnetic Compatibility (EMC).
-
Operate the forced cooling fan with all protective devices.
-
Following the operating instructions.
Related Documents
|
Title of Document |
Reference Number |
|---|---|
|
Pressure Relief Channel 1000 mm |
AGSC73700 |
|
Gas channel 1000 mm Anti Air Ventilating System (AAVS) Rear Exhaust |
PKR92704 |
|
Pressure Relief Channel 1000 mm AAVS Vent |
BQT10948 |
DANGER
WARNING