BRU8628300-00

Transport

WARNING
hazard of INAPPROPRIATE HANDLING
When transporting the fan, ensure that the units do not slip or tip.
Ensure that the specified transport temperature conditions are met.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
NOTICE
hazard of transport UNDER INADEQUATE CONDITIONS
Ensure that the specified transport temperature conditions are met.
Failure to follow these instructions can result in equipment damage.

Transport temperature conditions:

  • Maximum permitted ambient temperature for motor: + 80 °C

  • Minimum permitted ambient temperature for motor: - 40 °C

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?