BRU8628300-00

Reactive Currents

As the EMC filter complies with EMC limits (interference emission and immunity to interference), reactive currents can be measured in the supply line even when the motor is at a standstill and the line voltage is switched ON.

The reactive current values are typically in the range < 250 mA.

At the same time, the effective power in this operating state (operational readiness) is typically < 4 W.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?