BRU8628300-00

Condensator Wiring

NOTE: The starter condensators have to be fixed on top of the low voltage cabinet.

Follow the below steps to connect the condensator:

  1. Remove the four M6 x 10 bolts (4) and remove the plastic cover (1).

  2. Connect the two capacitor plugs (2) from the fans with the two condensator plugs.

  3. Reassemble the plastic cover (1) and install the four M6 x 10 bolts (4).

  4. Position the condensator assembly (3) on top of the LV box.

  5. Install the four M6 x 12 bolts (4) along with plain washers and lock nuts with spring washer on each side.

NOTE:
  • The below shown pictures are for representation only, and they may differ from the actual products.

  • In case of open delta resistor system in combination with condensator, contact Schneider Electric for assembly details.

Figure 7
Condensator Assembly

1

Plastic cover

3

Condensator

2

Capacitor plugs

4

M6 x 10 bolts

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?