BRU8628300-00

Mechanical Connection

WARNING
HAZARD OF INAPPROPRIATE HANDLING
Two personnel are required to remove the device from its packaging.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
CAUTION
CRUSH HAZARD
  • To avoid any shocks, carefully remove the blowers from its packaging only by touching the housing.
  • Comply with the electrical safety precautions. Refer to Safety Precautions.
  • Apply appropriate PPE and follow safe electrical work practices.
Failure to follow these instructions can result in injury or equipment damage.
CAUTION
HAZARD OF INAPPROPRIATE ASSEMBLY
Ensure that the device is securely positioned at its place of installation until all fastening screws have been tightened.
Failure to follow these instructions can result in injury or equipment damage.
NOTICE
HAZARD OF ABNORMAL USE CONDITIONS
Bearing damage can cause shorter service life:
  • Ensure there is no damage to the device from vibration.
  • Do not subject the fan to force or excessive vibration from sections of the installation.
  • Isolate the connection from vibration, if the fan is connected to air ducts, for example using compensators or similar elements.
  • Ensure that the fan is attached to the substructure without causing any stress or strain.
  • Check the device for transport damage. Do not install the damaged devices.
  • Install the undamaged device in accordance with your application.
  • The fan must not be strained on fastening.
Failure to follow these instructions can result in equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?