0611CT1603

Bare-cable connector

Conducting part of the circuit breaker intended for connection to power circuits. On PowerPacT circuit breakers, you can use Everlink lugs or copper/aluminum lug options that screw to the connection terminals of the circuit breaker. Connectors have one or more holes (single or multiple cable connector) for the ends of bare cables.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.