0611CT1603

EMC (Electromagnetic compatibility)

EMC is the capacity of a device not to disturb its environment during operation (emitted electromagnetic disturbances) and to operate in a disturbed environment (electromagnetic disturbances affecting the device). The standards define various classes for the types of disturbances. MicroLogic™ trip units comply with annexes F and J in standard IEC IE60947-2.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.