0611CT1603

Short-circuit making capacity (Icm)

Value indicating the capacity of the device to make and carry a high current without repulsion of the contacts. It is expressed in kA peak.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.