0611CT1603

Degree of protection against external mechanical impacts (IK)

Defines the aptitude of an object to resist mechanical impacts on all sides, resistance being designated by an identifying number set out by the listing standard. Each number corresponds to the impact energy that the object can handle according to a standardised procedure.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.