0611CT1603

Disconnector IEC 60947-3

"Mechanical switching device which, in the open position, complies with the requirements specified for the isolating function". A disconnector serves to isolate upstream and downstream circuits. It is used to open or close circuits under no-load conditions or with a negligible current level. It can carry the rated circuit current and, for a specified time, the short-circuit current.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.