0611CT1603

Make contact
IEC 60947-1

"Control or auxiliary contact which is closed when the main contacts of the mechanical switching device are closed and open when they are open".
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.