0611CT1603

Thermal release

Release in which a bimetal strip is heated by the Joule effect. Above a temperature-rise threshold that is a function of the current and its duration (I2t curve = constant, which is representative of temperature rise in cables), the bimetal strip bends and releases the circuit breaker opening mechanism. The pick-up setting may be adjustable.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.