0611CT1603

Reflex tripping

PowerPacT circuit breakers have a patented reflex-tripping system based on the energy of the arc and that is independent of the other protection functions. It operates extremely fast, before the other protection functions. It is an additional safety function that operates before the others in the event of a very high short circuit.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.