0611CT1603

Temperature derating

An ambient temperature varying significantly from 40°C can modify operation of magnetic or thermal-magnetic protection functions. It does not affect electronic trip units. However, when electronic trip units are used in high-temperature situations, it is necessary to check the settings to ensure that only the permissible current for the given ambient temperature is let through.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.